Grove Infrared sensor array

Can you give a some more details of the position resolution. I couldn’t work out from your video etc if the sensor has a lens and forms an 8X8 pixel image. If it has a lens, what is the resolution in degrees for each pixel?



Tony

Hi Tony

Temperature detection of two-dimensional area is 8 × 8 (64 pixels). For more, please refer to <LINK_TEXT text=“http://wiki.seeedstudio.com/Grove-Infra … y-AMG8833/”>http://wiki.seeedstudio.com/Grove-Infrared_Temperature_Sensor_Array-AMG8833/</LINK_TEXT>. For the datasheet, please refer to <LINK_TEXT text=“https://github.com/SeeedDocument/Grove- … /AMG88.pdf”>https://github.com/SeeedDocument/Grove-Infrared_Temperature_Sensor_Array-AMG8833/raw/master/res/AMG88.pdf</LINK_TEXT>. thanks.

Hi Bill



Thank you for the link to the Panasonic datasheet which has a useful diagram showing how the pixels are mapped.



Tony