How do I connect the Grove - Infrared Emitter to the Netduino Plus board? I tried both 3 and 5 volts on the Netrduino plus and connected TX to digital PIN 11. I passed an IR signal and looking through a camera, the LED was not blinking at all.
Marwan Shouery
Not sure about the netduino plus, any luck seeing people using it with Grove system? Thanks!
How much voltage does the Grove - Infrared Emitter need? I may be supplying a very low voltage. Marwan
it is 3.3V or 5V compatible.
maybe you can check:connct the Vcc and Tx pin to 5V source, and looking through a camera to see if the LED lighted.