Which kind of Seeeduino/Arduino board is compatible with Grove IMU 10DOF?
Could you please provide the board name and type?
Thank you!
Hello,
Seeeduino V4.2 is the latest version of Seeeduino board based on UNO bootloader will be compatible with IMU10DOF.
It also has an Grove I2C port in it which makes it easy to connect the grove IMU10DOF with the Seeeduino.
To know more about Seeeduino V4.2 please refer the following wiki page.
Thanks and Regards
Thank you!
Besides Seeeduino V4.2, is Seeeduino Lite or other board suitable?
Hi,
Yes,Any Seeeduino /Arduino with I2C capability can be used with grove IMU 10DOF.
Thanks and Regards
Hi,
is it possible to use two IMU-10DOF groves at the same time?
How?
It is possible to change the adress of the MPU unit with the jumpers. Is this possible for the BMP180 too?
I want to use them with a seeeduino 4.0, which only has one i2c-grove connector. The other one is a uart connector. Can I plug the second IMU-10DOF into the uart grove, or can I plug it into the scl/sca (+5V/gnd)PINs of the board, or should i use the grove hub?
A single IMU-10DOF works fine by the way, although it is hard to use the sensor fusion with ahrs on a little arduino.
Thanks a lot!
Hello,
Its not possible to use two IMU10DOF groves at the same time.
Changing I2C address of BMP180 is also not possible.
Thanks and Regards