Grove hat base for raspberry pi : compatibility

Hello,

I just started to use grove sensors on raspberry Pi 3b with a grove hat base for Raspberry.
It works perfectly with https://codeload.github.com/Seeed-Studio/grove.py/zip/master

My concern is about the exact list of supported grove sensors: the Grove Base Hat Compatibility List I founded on the web specifies sensors that are not provided with examples on the grove.py/master. eg: 101020073 Grove - Electromagnet 30/04/2014 Digital 5V √
or 101020452 Grove - OLED Display 1.12’’ V2 17/08/2017 I2C 3.3V/5V √

Could someone explain if these sensors are supported, and the corresponding libraries ?

Best regards !
RoboSkop

=>

Hi @RoboSkop, As per Seeed WiKi page, The Grove - Electromagnet and Grove - OLED Display mentioned that it’s compatible with raspberry pi, for code and demo please refer the wiki page.

Hi Salman, Thanks for your answer. But is there not a difference between grovepi and grove hat base for these components ? Do I use grove pi library with the grove hat base ?

Can you share the product link?

https://wiki.seeedstudio.com/Grove_Base_Hat_for_Raspberry_Pi/

:smiley:

Cool, You need to use Grove.py it’s a python library for seeedstudio grove devices on embedded Linux platform. you can find more details here: https://wiki.seeedstudio.com/Grove_Base_Hat_for_Raspberry_Pi/#archtecture