How do you enable 10hz and 115200 baud on the gps using the Arduino? I cant get it to communicate faster than 9600.
Hello, have you tried changing SoftSerial.begin(9600) and Serial.begin(9600) in your code?
Yep. If I switch to anything over 9600, it doesn’t work, no communication.
You change the baud rate of your code,and the baud rate of your serial monitor also needs to be modified accordingly
I’m aware. That’s been done already.
You can try to write a simple code to test whether your board UART can send and receive properly
It works at 9600. Need it at a faster baud rate and refresh rate.
Which MCU are you using? I might be able to try to verify and solve
Arduino Mega… appreciate it