Is the firmware for this Grove Module including the DSP algorithms - open source and if so where do I find them?
Sorry,the firmware is not opensource.We only provide the bin file to upgrade the firmware which is available in the wiki page.
can I use this sensor to calculate SpO2 -the oxygen rate in blood
What is the relationship between SpO2 -the oxygen rate and finger-clip Heart rate? @mhmoud_naes