Grove - Doppler Radar (BGT24LTR11) Issue

Received the doppler radar sensor. Very cool. Set up the test code on a Wio Terminal and printed speed through the serial terminal. Overall works good. However, speed values are not consistent. For example, moving a hand away from the sensor at a constant speed may give 52, 52, 104, 416, 364, 52… Not sure if this is typical or if my particular device has an issue.

I also created a display for the Wio Terminal with the current speed in mph, max speed and line graph. Had the same issue with inconsistent values. When testing the unit with a walker approaching the sensor, resulting values were around 3.5 mph but also included some error spikes between 5 and 11 mph.

FYI, the documents mention the speed is 52cm/s or multiples of (correct) or 2.23 mph (incorrect, should be 1.16 mph)

Appreciate any feedback. Thanks!

1 Like

It looks like you’ve done a great project. Can you share it with us?
You said the data is inaccurate.We can follow you to share further tests.

1 Like

FYI the speed 0.52m/s is approx 1.868 km/h.

1 Like