Grove Beginner Kit Lesson 10 Sensing Movement

I copied the code from the manual pdf and lesson 10 would not compile.

I installed the zip file to the library as instructed.

The error was Compilation error: ‘I2C_MODE’ was not declared in this scope

Here is the code:

//Gravity Acceleration
#include “LIS3DHTR.h”
#ifdef SOFTWAREWIRE
#include <SoftwareWire.h>
SoftwareWire myWire(3, 2);
LIS3DHTR LIS(I2C_MODE);//IIC
#define WIRE myWire
#else
#include <Wire.h>
LIS3DHTR LIS(I2C_MODE);//IIC
#define WIRE Wire
#endif
void setup() {
Serial.begin(9600);
while (!Serial) {};
LIS.begin(WIRE); //IIC init
delay(100);
LIS.setOutputDataRate(LIS3DHTR_DATARATE_50HZ);
}
void loop() {
if (!LIS) {
Serial.println(“LIS3DHTR didn’t connect.”);
while (1);
return;
}
//3 axis
Serial.print(“x:”); Serial.print(LIS.getAccelerationX()); Serial.prin
t(" “);
Serial.print(“y:”); Serial.print(LIS.getAccelerationY()); Serial.prin
t(” ");
Serial.print(“z:”); Serial.println(LIS.getAccelerationZ());
delay(500);
}

Hi,
Copying code from the PDF file will cause some problems like wrong punctuations. Here is the online version of the lessons where the code is easy for copying: