Grove Angles

Greetings

I am plying with one of these devices

http://wiki.seeedstudio.com/Grove-Servo/



First, the example for servo says to use D9, however, the base board only goes up to 8. I changed to a lower number and got it to work.



However, my real question is "Does this servo only range between 0 and 180 degrees?

Hi there, we updated the wiki, thanks for the feedback. the arrange is 0~180 degree. thanks.



Seeed techsupport team

Bill