Grove AI HAT and Maix camera cable

I would like to suggest either an extension cable, or a camera module with a cable which can be used with the Grove AI HAT, Maix Bit etc.



My reason is that the board can not always be located with the camera. It would also allow the camera to be used with gimbal bases for computer vision and robotics projects.

Hi,



Are you looking for a camera connector ?

Not exactly. The cameras used for the modules just have a short stub of ribbon. What I’m suggesting is a longer cable, not a ribbon. This is so the camera can be mounted away from the device, and even mounted on a motor controlled base if desired.



For example, I have a small mount made for FPV cameras I think. It has servos for yaw and pitch. Being able to use a base like that with a camera on a K210 board would be amazing for things like object tracking.