Happy New Year, everyone!
I’m sorry to start the year off with another problem…
I’m having issues setting up the 3-axis digital accelerometer (±1.5g) for a uni project I’m working on:
I’m running Raspian 10 on a Raspberry Pi 3 Model B Rev 1.2.
I installed the Grove Pi Software using
</s>curl -kL dexterindustries.com/update_grovepi | bash<e>
and updated the firmware.
After connecting the Grove 3-Axis Digital Accelerometer (±1.5g) to the I2C-1 Port and running the grove_i2c_accelormeter.py file in ~/Dexter/GrovePi/Software/Python the process gets stuck. Terminating through Control+C does not work and I have to close the Console to kill the process.
I have also attached the log generated by Dexter Industries’ “Test and Troubleshoot” Program.
I looked at it and while it says that it cannot find wiringPi and that I2C and SPI are still in the blacklist, I checked and the system both has the latest version of wiringpi and the /etc/modprobe.d/raspi-blacklist.conf file is empty.
While looking for a fix, I already enabled both I2C and SPI through raspi-config AND added
</s>dtparam=i2c1=on
dtparam=i2c_arm=on
dtparam=i2s=on
dtparam=spi=on<e> to my /boot/config.txt file.
journalctl also didn’t give me any direct clues on what’s wrong as there don’t seem to be problems with loading related modules.
I’d be super happy for any help I can get - as the final presentation date gets closer and closer
Thanks a lot in advance and best regards,
Lukas
log.txt:
Check space left
================
Dateisystem Größe Benutzt Verf. Verw% Eingehängt auf
/dev/root 15G 3,9G 9,7G 29% /
devtmpfs 459M 0 459M 0% /dev
tmpfs 464M 0 464M 0% /dev/shm
tmpfs 464M 13M 451M 3% /run
tmpfs 5,0M 4,0K 5,0M 1% /run/lock
tmpfs 464M 0 464M 0% /sys/fs/cgroup
/dev/mmcblk0p1 253M 53M 200M 21% /boot
tmpfs 93M 4,0K 93M 1% /run/user/1000
Check for dependencies
======================
python 2.7.16-1 install ok installed
python-pip 18.1-5+rpt1 install ok installed
git 1:2.20.1-2+deb10u1 install ok installed
libi2c-dev 4.1-1 install ok installed
python-serial 3.4-4 install ok installed
python-rpi.gpio 0.7.0~buster-1 install ok installed
i2c-tools 4.1-1 install ok installed
python-smbus 4.1-1 install ok installed
dpkg-query: Kein Paket gefunden, das auf arduino passt
dpkg-query: Kein Paket gefunden, das auf minicom passt
scratch 1.4.0.6~dfsg1-6 install ok installed
find: ‘/run/user/1000/gvfs’: Keine Berechtigung
wiringPi Not Found (ERR)
find: ‘/run/user/1000/gvfs’: Keine Berechtigung
I2C still in blacklist (ERR)
SPI still in blacklist (ERR)
Check for addition in /modules
==============================
I2C-dev already there
i2c-bcm2708 already there
spi-dev already there
Hardware revision
=================
gpio version: 2.50
Copyright (c) 2012-2018 Gordon Henderson
This is free software with ABSOLUTELY NO WARRANTY.
For details type: gpio -warranty
Raspberry Pi Details:
Type: Pi 3, Revision: 02, Memory: 1024MB, Maker: Sony
* Device tree is enabled.
*--> Raspberry Pi 3 Model B Rev 1.2
* This Raspberry Pi supports user-level GPIO access.
Check the /dev folder
=====================
i2c-1
spidev0.0
spidev0.1
ttyAMA0
USB device status
=================
Bus 001 Device 004: ID 05ac:0256 Apple, Inc.
Bus 001 Device 003: ID 0424:ec00 Standard Microsystems Corp. SMSC9512/9514 Fast Ethernet Adapter
Bus 001 Device 002: ID 0424:9514 Standard Microsystems Corp. SMC9514 Hub
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
/: Bus 01.Port 1: Dev 1, Class=root_hub, Driver=dwc_otg/1p, 480M
|__ Port 1: Dev 2, If 0, Class=Hub, Driver=hub/5p, 480M
|__ Port 1: Dev 3, If 0, Class=Vendor Specific Class, Driver=smsc95xx, 480M
|__ Port 4: Dev 4, If 1, Class=Human Interface Device, Driver=usbhid, 12M
|__ Port 4: Dev 4, If 0, Class=Human Interface Device, Driver=usbhid, 12M
Raspbian for Robots Version
===========================
cat: /home/pi/di_update/Raspbian_For_Robots/Version: Datei oder Verzeichnis nicht gefunden
Hostname
========
raspberrypi
Checking for Atmega chip
========================
avrdude: Version 5.10, compiled on Jun 18 2012 at 12:38:29
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
Copyright (c) 2007-2009 Joerg Wunsch
System wide configuration file is "/etc/avrdude.conf"
User configuration file is "/home/pi/.avrduderc"
User configuration file does not exist or is not a regular file, skipping
Using Port : unknown
Using Programmer : gpio
AVR Part : ATMEGA328P
Chip Erase delay : 9000 us
PAGEL : PD7
BS2 : PC2
RESET disposition : dedicated
RETRY pulse : SCK
serial program mode : yes
parallel program mode : yes
Timeout : 200
StabDelay : 100
CmdexeDelay : 25
SyncLoops : 32
ByteDelay : 0
PollIndex : 3
PollValue : 0x53
Memory Detail :
Block Poll Page Polled
Memory Type Mode Delay Size Indx Paged Size Size #Pages MinW MaxW ReadBack
----------- ---- ----- ----- ---- ------ ------ ---- ------ ----- ----- ---------
eeprom 65 5 4 0 no 1024 4 0 3600 3600 0xff 0xff
flash 65 6 128 0 yes 32768 128 256 4500 4500 0xff 0xff
lfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
hfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
efuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
lock 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
calibration 0 0 0 0 no 1 0 0 0 0 0x00 0x00
signature 0 0 0 0 no 3 0 0 0 0 0x00 0x00
Programmer Type : GPIO
Description : Use sysfs interface to bitbang GPIO lines
avrdude: AVR device initialized and ready to accept instructions
Reading | ################################################## | 100% 0.00s
avrdude: Device signature = 0x1e950f
avrdude: safemode: lfuse reads as FF
avrdude: safemode: hfuse reads as DA
avrdude: safemode: efuse reads as 5
avrdude: safemode: lfuse reads as FF
avrdude: safemode: hfuse reads as DA
avrdude: safemode: efuse reads as 5
avrdude: safemode: Fuses OK
avrdude done. Thank you.
Checking I2C bus for devices
============================
Checking I2C bus 0
==================
Error: Could not open file `/dev/i2c-0' or `/dev/i2c/0': No such file or directory
Checking I2C bus 1
==================
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- 04 -- -- -- -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- 4c -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --
Checking for firmware version
=============================
GrovePi has firmware version: 1.4.0
salman
January 12, 2020, 8:50am
2
Hi,
can you try the Accelerometer with an Arduino and make sure that the sensor working fine, then we can further followup the problem?