Grove 2-channel inductive sensor example sketch on arduino IDE LDC1612

Hello,
I’m facing the stray error issue while trying to compile the LDC1612 coin example. I tried clearing any spaces and auto formatted the code multiple times but nothing seems to help. I also tried to copy paste the code from your website but the stray error continues. I further tried to use the arduino web editor but that too hasn’t helped. Could you please help me fix this?


I have compiled it here with no problems, what development board are you using?

I’m using arduino UNO. Do you mind copy pasting your code here?

My code is exactly the same as yours, but I compiled it with Wio Terminal.

#include "Seeed_LDC1612.h"
 
LDC1612 sensor;
const u32 DISTANCE_00=44000000;  //do not detect
const u32 DISTANCE_00_01=60000000;  // distance:<1mm
const u32 DISTANCE_01_05=45000000;  // distance:1mm~5mm
const u32 DISTANCE_05_10=44250000; // distance:5mm~10mm
const u32 DISTANCE_10_15=44080000; // distance:10mm~15mm
const u32 DISTANCE_15_20=44020000; // distance:15mm~20mm
 
void setup()
{
    Serial.begin(115200);
    delay(100);
    Serial.println("start!");
 
    sensor.init();
 
    if(sensor.single_channel_config(CHANNEL_0))
    {
        Serial.println("can't detect sensor!");
        while(1);
    }
 
 
}
 
 
void loop()
{
    u32 result_channel1=0;
    u32 result_channel2=0;
 
    /*shows the status of sensor.*/
    //sensor.get_sensor_status();
 
    /*Get channel 0 result and parse it.*/
    sensor.get_channel_result(CHANNEL_0,&result_channel1);
 
    /*Test the distance between the coin and the sensor. 
    Note that the accuracy is for reference only.
    Please suspend the sensor during the test! */
    if(0!=result_channel1)
    {
        if(result_channel1<DISTANCE_00)
        {
            Serial.println("There is no coin here!");
        }
 
        if(result_channel1>=DISTANCE_00_01)
        {
            Serial.println("The distance between the COIN is 0~1mm");
        }
 
        if(result_channel1<DISTANCE_00_01&&result_channel1>=DISTANCE_01_05)
        {
            Serial.println("The distance between the COIN is 1~5mm");
        }
 
        if(result_channel1<DISTANCE_01_05&&result_channel1>=DISTANCE_05_10)
        {
            Serial.println("The distance between the COIN is 5~10mm");
        }
 
        if(result_channel1<DISTANCE_05_10&&result_channel1>=DISTANCE_10_15)
        {
            Serial.println("The distance between the COIN is 10~15mm");
        }
 
        if(result_channel1<DISTANCE_10_15&&result_channel1>=DISTANCE_15_20)
        {
            Serial.println("The distance between the COIN is 15~20mm");
        }
 
        if(result_channel1<DISTANCE_15_20&&result_channel1>=DISTANCE_00)
        {
            Serial.println("The distance between the COIN is more than 2mm");
        }
 
    }
 
    delay(1000);
}

I have also tested it with Arduino UNO and it compiles with no problem. Attached is the code.