Hi all!
Just curious if the Grove 125KHz RFID module (RDM630) [1] can write onto writable tags as well? If yes, would it be as straightforward as SoftwareSerial.write() via UART TX/RX? If not, please feel free to suggest another module.
[1] https://www.seeedstudio.com/125Khz-RFID-module-UART.html
P.S . I can successfully read tag info using this module with Arduino.
@user3248648749 I think the key to this question is whether your TAG can be written.Because a lot of tags are read-only.
I get that, I am talking about the re-writable ones (eg - T5577). Even with that will it be possible?
I think it is ok, of course, there are many incompatible factors, need to test to know. @user3248648749