Hi, I have bought the Grove - 125KHz RFID Reader and I need to use it with Arduino UNO.
I just receive “RFID Test…” message in my monitor serie of Arduino UNO (also with TEST and DEBUG on), the tag that I am using is the typical EM4100 125khz RFID Key (RFID Tag). I am sure that reader is working because when I approach the tag key the green led lights, so, is detecting the RFID Tag but it doesn´t read it.
Is there anything I can do?
Do this RFID reader works only with cards?
Thank in advance