Hello,
I’ve a seeeduino stalker 2.b, and I’m not able to use a gps bee module, neithe in the bee slotnor using a shieldxbee.
What I have to do to let him run?
Thanks!
MArco
Hello,
I’ve a seeeduino stalker 2.b, and I’m not able to use a gps bee module, neithe in the bee slotnor using a shieldxbee.
What I have to do to let him run?
Thanks!
MArco
no opinion? here my code:
[code]/*
Program that read a char from serial port and turn on a led (pin 13)
if the char was H. Put it low is the char is an L
*/
/* parallax code */
//int ledPin = 13;
#include <Wire.h>
char string[32];
char byteRead;
int ledPin = 13; // LED test pin
int rxPin = 0; // RX PIN
int txPin = 1; // TX TX
int byteGPS=-1;
char linea[300] = “”;
char comandoGPR[7] = “$GPRMC”;
int cont=0;
int bien=0;
int conta=0;
int indices[13];
/------------------------------------/
void setup() {
// initialize serial communication:
Serial.begin(9600);
/* parallax code */
for (int i=0;i<300;i++){ // Initialize a buffer for received data
linea[i]=’ ';
}
// initialize the LED pins:
// pinMode(ledPin, OUTPUT);
}
void loop() {
digitalWrite(ledPin, HIGH);
byteGPS=Serial.read(); // Read a byte of the serial port
if (byteGPS == -1) { // See if the port is empty yet
delay(100);
} else {
linea[conta]=byteGPS; // If there is serial port data, it is put in the buffer
conta++;
Serial.print(byteGPS, BYTE);
}
} [/code]
Thanks!
No support for this Item? 
How is the gps bee thing supposed to be connected anyway? In another thread someone is trying to use NewsoftSerial to talk to gps on pins 11 and 12 if I remembe correctly…
Yes, GPSbee can work with Stalker v2.0.
Thanks
Albert