I’m working with the GPRS Module V2.0, but i’m having problems with the power, I’m using the module to send data via ftp to a server sending data each hour, I’m using an Arduino Mega 2560 board, when I use a charger ([email protected]) it works great, but when i use a rechargable battery (12V@7Ah) with a regulator (L7805CV - 5V @ 1A) it works for a couple of hours and then it drains all the battery. So what kind of power its required by this module?
Hello
I think you have solved your problem since last year but I used shield :
seeedstudio.com/depot/Energy … cPath=1_75
and Li-on battery
seeedstudio.com/depot/Polyme … ?cPath=1_3
and no problem for battery
On my side I have problem for send file by ftp from my sd card , can you show your code ?
Thanks
Hello tabanou 
I have a similar problem. Did you find a solution to your problem? Any example code?
regards