GPRS Shield1.2 and FEZ Domino reboots sending data over GPRS

I’m using the GPRS Shield 1.2 and the FEZ Domino to GET or POST data to a website over GPRS. I’ve used both the GPRS commands and the embedded HTTP commands for communications. Both methods work well.

However, sometimes while communicating, the GPRS shield causes the FEZ Domino to reboot.

I’m using a 9V 3A power supply which should provide plenty of power to the FEZ Domino and the GPRS shield.

What might be the problem?

Oh…

I think there could be a poor contact in hardware.

Or the GET would exception.The libraries is not very stable, that could be happen like this.

Hope can help you.