GPRS Shield + Xbee Shield + Xbee module + Arduino UNO

Hi,

Is it possible to use the GPRS module for controlling one arduino via SMS? That arduino must also have the possibilty of wireless communication with another Arduino uno using xbee modules. The GPRS Arduino should receive commands of switching and send some information (digital input status) via SMS.

Summing up:

Arduino 1 + GPRS + Xbee (receive via SMS, transmit/receive via Xbee to/from Arduino 2)

Arduino 2 + Xbee (transmit/receive via Xbee to/from Arduino 1)

Regards,

Jorge

In function, it is possible, but in physical, you may need to figure out how to connect XBee as well as GPRS Shield on Arduino.
Maybe you need Bees Shield:http://www.seeedstudio.com/depot/bees-shield-p-672.html?cPath=109