Hi
Wanting this shield to go in a sculpture and to always be one when the arduino is on. So if i have a power cut or someone un plugs then when it gets plugged backend it will automatically start up again. Two options that I thought of
- solder the switch to be on all the time.
- solder the switch so that I can controlled it from the arduino board.
Of course 1) is easier but I don’t really understand if this a good thing or not. Don’t want to blow things up or have it not start. Anyone done this or have advice around how to do this?
cheers Paul