Hello,
is it possible, that the GPRS Shield switch a GPIO Pin to high if the network connection is lost?
The GPRS Shield must do this action in case that the microcontroller board ( arduino ) is crashed or currently under an heavy calculation and not able the send an AT Command to the GPRS Shield to establish if the connection to the network is true.
kind regards
dieter