GPRS on Arduino Uno pins

I would like to know exactly which connections are to be made between “Arduino one” and gprs shield v2.0.
This is because I built a Arduino one and I want to connect the shield GPRS, using only the pins that are needed to shield.
Using the software serial so I assume pin D7, D8, D9 for reset, GND and VIN.
Some other connection?
I do not need the serial hardware.

I state that I have already used the shield with the board “Arduino one” original and everything works perfectly.
thanks

That’s enough, you don’t need other connections. More information you can refer to it’s schematic.