GPIO pins not responding in code

Hello.

I’ve been stuck all day trying to get any of the GPIO pins to change state from a small python script.

I followed the example in the wiki, and the IRQTest.py just said false with every loop (ran as root).

I used this library https://github.com/vsergeev/python-periphery that is also in the IRQtest.py with this code:

import time
from periphery import GPIO

gpio = GPIO("/dev/gpiochip0", 40, "out")
gpio.write(False)
time.sleep(1)
gpio.write(True)
time.sleep(2)

gpio.close()

Basically, I am trying to activate a relay.

The pin stays at 1.38 volts while the script runs (as root). I’ve tried /dev/gpiochip1 as well, no change.

I can change the pin state in the bios, and when I set it to low, the pin reads at .03 volts. So I think the GPIO pins themselves are fine. I am stumped as to why doing anything from linux just doesn’t work.

I tried Debian 10 and Fedora 32

Thanks

Some more digging on my end…
I am trying to use libgpiod, which accesses the gpio pins through a character device. The sysfs method is deprecated and removed in newer kernels, so everybody is going to have to adjust anyway.

See https://git.kernel.org/pub/scm/libs/libgpiod/libgpiod.git/about/

So, what I am now essentially asking is…What is the correlation between the physical pin number and the line number? 4 gpiochips show up, and 0 and 1 both have 80 lines.

# gpiodetect
gpiochip0 [INT3453:00] (80 lines)
gpiochip1 [INT3453:01] (80 lines)
gpiochip2 [INT3453:02] (20 lines)
gpiochip3 [INT3453:03] (35 lines)

Which gpiochip is the 40 pin setup on the board?

gpioinfo
gpiochip0 - 80 lines:
	line   0:      unnamed       unused   input  active-high 
	line   1:      unnamed       unused   input  active-high 
	line   2:      unnamed       unused   input  active-high 
	line   3:      unnamed       unused   input  active-high 
	line   4:      unnamed       unused   input  active-high 
	line   5:      unnamed       unused   input  active-high 
	line   6:      unnamed       unused   input  active-high 
	line   7:      unnamed       unused   input  active-high 
	line   8:      unnamed       unused   input  active-high 
	line   9:      unnamed       unused   input  active-high 
	line  10:      unnamed       unused  output  active-high 
	line  11:      unnamed       unused  output  active-high 
	line  12:      unnamed       unused  output  active-high 
	line  13:      unnamed       unused   input  active-high 

From other pages I’ve seed, the broadcom chips have labels. And there is no correlation between pin number and line number. I’ve already caused a crash and reboot by setting line 47 to high.

I did some trial and error and nailed down the chip and line number of a few pins using a relay and patience.

I then stared at the numbers in the bios for the pins and realized there is a pattern.

Here are my results, most of them checked by hand using the gpioset utility.

bios_number physical_pin chip_number line_number
60 10 0 60
61 8 0 61
79 23 1 3
80 24 1 4
81 26 1 5
82 21 1 6
83 19 1 7
88 11 1 12
110 3 1 34
111 5 1 35
112 27 1 36
113 28 1 37
114 22 1 38
115 32 1 39
134 36 1 58
136 13 1 60
137 15 1 61
139 29 1 63
140 31 1 64
141 33 1 65
143 37 1 67
145 16 1 69
146 18 1 70
161 7 2 5
162 12 2 6
163 35 2 7
164 38 2 8
165 40 2 9

Now, going back to my original snippet, I see that physical pin 40 (off in the far corner :stuck_out_tongue:) is on /dev/gpiochip2 on line 9. And now it works as expected!

If at somepoint Ubuntu or Debian finally drops GPIO sysfs, I hope someone googling around sees this post. Or if you are using Fedora IoT right now.

I’ll probably make a fork of python-periphery to integrate this mapping more easily, so you only have to worry about the physical pin layout number.

Thanks @zerrofour4 for the good work!

This is very useful for other users to see. :smiley:

Thanks so much for this @zerrofour4, saved me a lot of time and frustration :smile:

Thank you for the fine detective work. I just started looking into the GPIO thing on the Odyssey definitely saved me some work by posting your findings

GPIO sysfs stil exist, just the numbers changed, just add 512 to every number.

Confirmed that GPIO sysfs works with 512 added to every number.
e.g.
pin on connect 28 → BCM1_ID_SCL which is 389 in your program, now works as 901.
see seeed odyssey pin overview for the other numbers

#define IO_PIN_ENABLE_3point3V 901 //389 // connector pin 28 for EN258 pcb

Hi there,
I think you need some delay’s in there.

gpio = GPIO("/dev/gpiochip0", 40, "out")
Delay (500);
gpio.write(False)
Delay (500);
time.sleep(1)

HTH
GL :slight_smile: PJ