Getting LSM6DS3 to Work on XIAO MG24 Sense with Gecko SDK (I2C)

Just wanted to follow up on this in case anyone else runs into a similar issue.

As it turns out, the problem was due to a mismatch in the I2C pin definitions — the SDA and SCL were swapped. Big thanks to @grobasoz for spotting the issue!

For anyone using the XIAO MG24 with the Arduino framework: the comment for the I2C pin definitions might be incorrect, which I had used as a source. According to the official XIAO MG24 schematic (KiCAD PDF), the correct wiring is:

#define SL_I2CSPM_I2C_PERIPHERAL      I2C0
#define SL_I2CSPM_I2C_PERIPHERAL_NO   1
#define SL_I2CSPM_I2C_SCL_PORT        gpioPortB
#define SL_I2CSPM_I2C_SCL_PIN         3
#define SL_I2CSPM_I2C_SDA_PORT        gpioPortB
#define SL_I2CSPM_I2C_SDA_PIN         2

Thanks again, @grobasoz — your help saved me a lot of time! :grin: