Hello…
I have a gateway on TTN…It is communicating…I have a Lora-e5 Module that I can send AT commands to over UART…I requested over UART and copied the DevEUI and AppEUI into the DevEUI and JoinEUI respectively on TTN. I generated a AppKey on TTN and copied that into the Lora - E5 module using the UART command…All looks good…I registered it but I do not see it showing up. I have chosen the correct freq…NAM1 and US915(TTN).
I now look at the TTN and the AppKey is different than what I copied over to my device…Is this correct or should it be the same? I also notice the Device Address (shortened version ) is not what the node shows me when I request it over the UART…is this a problem?
Should I delete application and try again? Thoughts?