Hi,
I have got the GPRS shield working great but what I want is to get the caller id when a button is pushed during a call then hang up below is the code I have so far
[code]
boolean stateChange=false;//used to check if button state has changed since last trigger
int lastState;//used to hold last state
void setup()
{
Serial.begin(19200);  //Default serial port setting for the GPRS modem is 19200bps 8-N-1
///////////////Turn GPRS on ////////////
pinMode(9, OUTPUT);
digitalWrite(9,LOW);
delay(1000);
digitalWrite(9,HIGH);
delay(2500);
digitalWrite(9,LOW);
delay(3500);
///////////////////////////////////////
Serial.write(“ATS0=3\r”);//answer after 3 rings
Serial.write("\r");
delay(1000);                    //Wait for a second while the modem sends an “OK”
/*Serial.write(“AT+CMGF=1\r”);    //Because we want to send the SMS in text mode
delay(1000);
}
void loop()
{
char number;//used to store caller id when D6 button pressed
int val6= digitalRead(6);//read state of D6 pin
int currentState=val6;//load state of D6 into currentstate to test for change
//perform action below if the current state has change from the laststate
if(currentState != lastState){
//Check if D6 is high
if(val6==HIGH){
Serial.write(“AT+CLIP?\r”);//request caller id
number=Serial.read();//read caller id and store in number variable
Serial.print(number);//print caller id
delay(2000);//wait 2 seconds
Serial.write(“AT+HVOIC\r”);//hang up
}
lastState=currentState;//store current state in last state variable
delay(10000);//wait 10 secs before beginning test again
}
}[/code]
The hanging up works ok so the code is being run ok when the button is pressed I am just not sure how to get the caller id to print in serial monitor.
If anyone has any ideas i’d be very grateful
Thanks in advance