What is the difference between Seeed’s Funnel IO Remixed vs the regular Funnel IO?
They are mostly the same. except the color!lol
And the price, I guess, too!
$5 less is a pretty good deal if they are essentially clones.
Thanks for the input!
Essetionally all the same. Please note that there are some peripheral modification:
- The 2 pin JST connector is remixed to 2.54mm from 2.00mm
- The TX/RX pin out is remixed to be compatible with UartSB v2.1