I am interested in making a prototype PCB incorporating the FPC breakout board which I just purchased. However, since I’d like to have it fit on the first try, can you provide a dimensional drawing or dimensions for the header spacing?
The header spacing is 0.5mm, total 60pin, thanks.
I understand the pin spacing is standard .5mm but I need the spacing between the two double row headers as well as the spacing between the front header and side header. I cannot make a prototype PCB to accept this adapter without this information.
Sorry for misunderstanding, here is the source file including 100% scale printed pdf. I have insert it into the product page too.
Thank you so much this is perfect! I will keep you posted with my results!