firmware updater stuck with error 1011

Hi all,
I just be starting with Link It One.
After the error I missed the 2 COM ports that are assigned to Link It.
How do I get it back?
Thanks
Regards,
Fred

additional info:
I am running Windows 7 Ultimate
I did also try running as administrator.

The updater stops at 5% download every time.
The message is “Failed! nError Code:1011”

I hope this info helps

Hi, please send me a email: [email protected], I will send you another factory tool to update the firmware, thanks~

Hi Loovee,
My 2 MTK USB Ports(Debug and Modem) are operational now.
For details see:
labs.mediatek.com/forums/posts/list/143.page
Best reagrds,
Fred