Hi,
I tried to update the Grove UART Wifi V2 AT firmware to the latest 2.2 release without success.
I ended up messing up with chip firmware, and now my board is bricked.
I tried to restore the firmware by using the procedure described here: Grove - UART Wifi V2 - Seeed Wiki
However, the device refuses to boot:
Is there someone that can confirm me the firmware available on the Seedstudio wiki works correctly even with the ESP8285 in V2 of the Grove-UART board?
I finally fixed the board by setting up the ESP8266-RTOS-SDK toolchain and by compiling the ESP-AT 2.2.0 release.
If interested in updating the Grove-UART WiFi V2 firmware, you can refer to this post on my blog