**Finally!**😛 Module for Seeed Studio XIAO - UART Interface, mini GPS/Tracker...more

:stuck_out_tongue: Finally!!
GNSS add on Module for Seeed Studio XIAO - UART Interface, mini GPS/Tracker,
Powered by Quectel L76K

Just showed up , Back ordered…LOL
Now we know where is Carmen Sandiego :smiley: :+1:
Check it out now…

Now we Are rolling.! NEXT a 3G Xiao… C’mon man.
GL :slight_smile: PJ :v:

Yes a large and heavy ceramic plate antenna helps the GPS reception, but it does not really make for a ‘mini’ GPS tracker.

With such a board, how would you actually receive the tracker location ?

Is that a XIAO with header pins pre-souldered or are they just teasing me?

Hi there,
Not sure How much you know about :satellite:GNSS GLOBAL GPS , It’s not your :artificial_satellite:GPS in your Phone :face_with_peeking_eye:. It is unlike any B4 it, Tiny :pinching_hand: by GNSS standards.
Compared even to the Demo I have on here for the Air530… This thing is perfect.
The antenna is of higher quality too.
The Real Question is what the current Draw? , How much power will it use.
They offer some software app, but a roll your own approach is what I’ll do.
So fantastic that it’s the same size as the XIao… I’m stoked.! :star_struck:

GL :slight_smile: PJ

Looks like the GPS is designed to be soldered to the back of the XIAO.

There are some details on the power consumption of GPSs here;

And how the type of antenna affects fix times here;

Note from the above that even a simple bit of wire, light and compact, can work quite well on the Quectel GPSs.

Power consumption of that GPS (Quectel L76) will be in the order of 15-25mA whilst aquireing a fix, typically 45 seconds, and it may settle down to 10-15mA after a couple of minutes.

For a lot of tracker applications then the GPS is normally run in ‘hot fix’ mode, after it gets a fix its powered down or put into standby and as long as there is a voltage on the battery backup pin the GPS maintains the satellite empherisis data it has downloaded and when powered back up will aquire a fix in 5 seconds or so and you can then power down again.

The L76 shown has a software backup current of 500uA and down to 7uA if you can power it down via a MOSFET etc. The L76 (allegadly) has a mode whereby it adapts to how its being moved around, when moving in a car say, it uses more power to maintain fix accuracy and can reduce power when its stationary or moving slowly. Quectel claim the power consumption can fall to 2.6mA.

Just seen this in the datasheet for the GPS;

Standby current OK, but that active antenna must be consuming a fair bit of current …