Cant see to find any info on interfacing to the WizFi250 via the SPI. Doc says you can, the libraries don’t have any apparent support although #define spi_CS 8 suggest something.
Any information so I can write direct support via SPI for commands and data is appreciated.
We only support UART interface. The default WizFi250 firmware only supports UART. We have libraries / examples for UART in Wiki.
WizFi250 module supports SPI by when firmware is updated.Read module documentation. It requires some hardware modification (Please see the schematic of the board. Not every SPI pin is already connected)