Fatal error when include <EEPROM.h>, develop using Arduino IDE

Hi Friends,



I have bought a Wio LTE Tracker.

I am going to use Arduino EEPROM methods, but when I add #include <EEPROM.h> and compile the sketch in Arduino IDE, I get error:



"

C:\Wio LTE\Library\Wio_LTE_Arduino_Library-master\examples\MyDevice\MyDevice.ino:7:20: fatal error: EEPROM.h: No such file or directory



#include <EEPROM.h>



^



compilation terminated.



exit status 1

Error compiling for board Wio Tracker LTE.

"



Could you please help me to find a good solution?

I have the same issue …

Jean-louis

Hi:

The EEPROM.h is compiled for Arduino/Genuino UNO and so on ,these boards use AVR chips.BUT the Wio LTE Tracker boards use STM32F4 chip,so you can not include EEPROM.H in your Wio LTE Tracker project.