I have been trying to get a FAT 32 implementation so I can use the only card I have, a 16G card, to work with a gps library for time and position. The goal being position and temperature logging to a text file or set of files that I can read on other systems. Unfortunately all my attempts to combine implementations FAT32 and NEMA parsing do not fit. I can get within 1k, but no closer. Has anyone succeeded in doing this or a similar task? What libraries did you use?
I use :
code.google.com/p/fat16lib/
and
code.google.com/p/sdfatlib/
from Bill.Greiman with arduino mega… and work ok.
i havent tested on stalker…
if you test it, please post a comment with results.
If you find a code that using SPI interface and support , that the stalker can support the FAT32 either . Now we provide the code that is a not a fully file system and just a filelogger demo , so it just support FAT16 and appending data into a existent file.
I have gotten to within 1k of fitting, but no better
I hate 168s…
Stalker with 168 will get extincted …soon.