How can I add another WS2813 60 RGB LED strip in DATA_PIN 3 to the code below?
code:
#include <FastLED.h>
#define NUM_LEDS 60
#define DATA_PIN 2
CRGB leds[NUM_LEDS];
void setup() {
FastLED.addLeds<NEOPIXEL, DATA_PIN>(leds, NUM_LEDS);
}
void loop() {
FastLED.setBrightness(100); // Set brightness to half of the max. (max. 255)
for(int i = 0; i <= NUM_LEDS-1; i=i+1) {
leds[i] = CRGB::White; // Set single LED to white
FastLED.show();
}
}