Factory reset of SenseCAP M2 (Helium version aka Light hotspot) make it uselesss

When using a SenseCAP M2 Light Hotspot LoRaWAN gateway (Helium hotspot) (M2-US915) the device will never receive the software update even though is connected to the internet. We’ve tested in several Internet connections, via ethernet and wifi, and I’ve read in Discord that there are 3 more people with the same issue. The top led indicator remains in solid white which means the unit is only with the factory firmware but it never loaded the exact same settings as it came out of the box, it has less features. Already created a support ticket but still the issue has not been solved.

Originally it came with:
Powered by LuCI / OpenWrt 21.02.0 r1-20220322 r16279-5cc0535800
System:
Model M2-US915
Build Version r1-20220322
OS Version 0.9.24-27
Firmware Version v1.0.0-alpha.23.3-23
helium_gateway Version 1.0.0-alpha.23
Helium Address *********key (3word animal name)
LoRaWAN Region US915

After factory reset it lost several modules in LuCi console and it shows:
Powered by LuCI / OpenWrt 21.02.0 r1-20220322 r16279-5cc0535800
System:
Model M2-US915
Build Version r1-20220322
OS Version 0.9.24-27
Firmware Version –

2 Likes

thanks for posting, i see you posted on the discord too… I cannt help because i have no knowledge, but i will say that the staff is out for weekend break and should be back around 9PM EST… maybe they will be able to help you… what on earth possessed you to do a factory reset… were you coned by a scammer?

I totally regret doing it, but the instructions said do not try to onboard it to Helium console if it has old firmware, so I unboxed it, and connected to internet. After several hours it didn’t update so I thought maybe resetting to factory will trigger a download of new firmware which is the expected behavior I see, but for some reason this version of M2 loses capability of downloading the latest.

Hi @Jessie1_SenseCAP here are some images of the limited menu that is available after factory reset.


Hi guys,

Happened the same to me.

I got the M2 gateway like two weeks ago and couldn’t onboard to helium due a Bluetooth error. Waited 2-3 days for the gateway to auto update itself to the latest firmware but that didn’t happen, it got stuck on 1.0.0-alpha.23
Navigating by the menus I find the option to factory reset my gateway and continue the process, hopping that by doing this the gateway could now update to the latest firmware and continue the onboarding process as normal, but that didn’t happen, now the hotspot does not displays a firmware version.

I reached for help on discord and this is how I got to this forum. Also I opened a ticket with the support team, but so far they only ask about my internet connection and stop replying more than 4 days ago.

I don’t know why it is such an issue to provide us with the firmware and let us flash the equipment by ourselves, many other brands provide it. I does not need to be the latest firmware, but only one that allow the gateway to connect to the server and initiate an OTA update.

I own another M2 Light hotspot that I bought last year and don’t have this issue at all, it came from the chinese warehouse not the US one, don’t know if that makes a difference.

Please help us solve this issue.

2 Likes

The bug has been fixed yesterday and now the device has been updated to latest firmware. The top led indicator is green now. I’ve read that the other 4 people with the issue have confirmed that it updated itself. The Helium LoRaWAN capabilities and the other parts of the menu has been restored.
Special thanks to the engineers, staff and other stakeholders who helped to fix it!

System

Hostname SenseCAP
Model M2-US915
SN *****
Build Version r1-20230423
OS Version 1.0.9-38
Firmware Version v1.3.0.2-48
helium_gateway Version 1.3.0
Helium Address ****** (animal-name-3words)
LoRaWAN Region US915
IMEI –
ICCID –
LTE RSSI –
GPS –
Local Time 2024-06-21 12:29:28 (America/CST)
Uptime 3h 32m 37s
Load Average 0.58, 0.52, 0.55

Powered by LuCI / OpenWrt 21.02.0 r1-20230423 r16279-5cc0535800.



For the record, this was the button that I used to factory reset my device. I hope you never have to use it, and if you do, I hope the expected behavior succeeds: automatic firmware upgrade.


Sorry guys, this is a known issue, we just fixed it 2 days ago and it should work now.

1 Like

How was this solved? I have the exact same issue where I reset my system to factory defaults and now I have the same limited menu.

|Model|M2-US915|
|Build Version|r1-20220615|
|OS Version|0.9.4-5|

Hi there,

And Welcome Here…

It was a undocumented enhancement :grin: (a.k.a. bug)
It will update itself after 24 hrs.

HTH
GL :slight_smile: PJ :v:

Thanks, @PJ_Glasso. Would be good if Seeed included this in the manual (in case someone from there is looking at this thread) =)

1 Like

The Sensecap M2 has been up for 24 hours and it hasn’t updated. Occasionally, I see the orange light turn on for ~2 seconds and then switch back to white.

Hello, i have the same problem (thouht pressing the button for about 30 seconds will give me the factory conditions…)

so do i get everything right: (i want to flash another firmware to the device)

i have to connect it to the internet (the device has to get ip adress vial lan / dhcp) and then i have to wait about 1 oder 2 days, and after that time (automatic update is over) i get the menu back for firmware update / to change the firmware?

thanks in advance

Solved: i flashed a different Firmware using a serial USB connection

2 Likes

Can you tell us more about how you did that? Where did you find the firmware image?

1 Like

alot of these things the update firmware is not needed… many scammers tell you to do this and redirect you to a scam site… especially if ith has to do with helium and cryp stuff… there is not much that can go wrong with these firmware… mainly because they dont update the firmware typically when it come seeed stuff

first i flashed this firmware: (via web admin in browser)

bit.ly/4ooCWd1

bit.ly/4741jWc

in my case i used the 868 one (EU) after this step you can, again, connect via wifi-AP with a default Wifi PW, then i flashed the firmware from the chirpstack website:

bit.ly/4qcEHLM

this works good for me, tried it with 3 devices now, and i am able to integrate this 3 devices in my chirpstack environment

as i thought that i bricked the device, i followed this guide (with teraterm-5.5.0-x64) which is really slow, it needed about 30-40 mins. to flash over serial-usb connection:

bit.ly/4qc5BDy

if you have further questions, you are welcome to ask me :slight_smile:

2 Likes

Thanks a lot @c0mm4nd3rk33n !

Eventually, which fw are you using? Is it usable for the helium network or just as a LoRaWan gateway?

i am using the chirpstack “chirpstack-gateway-os-4.9.0”, i am not sure about Helium, becaus we provide an local application with a local chirpstack server and node-red to convert our lora-data

as a private use-case i will try TTN in the future to provide my gateway to neighbors / locally

1 Like

i dont like that firmware updates take so long and they dont give any feedback on progress… its a mess…