External power to the 5V pin does not work for XIAO ESP32-S3 and XIAO ESP32-C3

Hi there,

And Welcome here..

So, On XIAO boards, the EN pin typically uses a weak pull-up (100 kΩ–1 MΩ) with a small C (~0.1–1 µF). When VBUS ramps slowly (e.g., from a spinning turbine), this:

  • Causes partial EN activation,
  • Powers the chip partially (warm to touch),
  • But fails to start properly.

Unfortunetly you can’t have it both ways as built.

Use a Soft Power-Up Supply (e.g. Supercap + Fast Diode + LDO)

Design your power circuit so that:

  • A Schottky diode charges a supercapacitor or large ceramic cap from the turbine.
  • Then feed that into a low dropout regulator (LDO) with a Power-Good (PG) pin.
  • Use PG to gate the LDO or control a switch to 3.3 V rail or USB port.

This ensures the LDO doesn’t output until it sees steady voltage is one way to do it that I know works.
I have used a small power bank in between the Charge cable and powered it with a solar panel power mc4 input, for example.

HTH
GL :slight_smile: PJ :v:

When you insert a USB power bank or regulated USB device between your turbine and the XIAO, it:

  1. Buffers the input voltage from the turbine’s ramp-up (slow/dirty 5V).
  2. Provides a clean, regulated 5V USB output to the XIAO.
  3. Holds enough internal charge to avoid brownouts on minor dips.
  4. Effectively delays VBUS rise seen by the Xiao until it’s stable.

:light_bulb: This “virtualizes” the power-up curve and mimics the stable power expected by the ESP32’s internal EN circuitry.