Ethernet Shield not working with Grove Shield

Hi Folks,

I am trying to run the Ethernet shield with the Grove Shield.

When the Grove Shield is not connected, the Ethernet shield works correctly.

But when the Grove Shield is attached above, Ethernet stops working.

Are folks able to run both of these shields at the same time? They “fit” and it looks like they should work together.

Thanks!

Hardware:
Azure Sphere MT3620 Development Kit_US Version
MT3620 Ethernet Shield v1.0
MT3620 Grove Shield
Azure Sphere OS: 21.07 Update 1
Azure Sphere SDK: 21.07.2.14662