Ethernet Shield clearance - or lack of it

Just got the Ethernet shield plugged into the Arduino Duemilanove and found that one of the Ethernet socket grounding/connection pins touches the top of the Arduino’s USB socket. No problem as they are both the same ground, but still…should really be moved over a couple of mills as I cant push the boards firmly together.
Ive got the 1.1 Ethernet shield from Seeed

Cheers

Mat

most of the time in that situation with shields (fairly common) just put some electrical tape around the usb plug and call it a day.