esp32S3 XIAO with round touch screen (seeedstudio) does not display anything

Hello,

in file TFT_eSPI/User_Setup.h, I have uncommented following lines

// ###### EDIT THE PIN NUMBERS IN THE LINES FOLLOWING TO SUIT YOUR ESP32 SETUP ######

// For ESP32 Dev board (only tested with ILI9341 display)
// The hardware SPI can be mapped to any pins

#define TFT_MISO 19
#define TFT_MOSI 23
#define TFT_SCLK 18
#define TFT_CS 15 // Chip select control pin
#define TFT_DC 2 // Data Command control pin
#define TFT_RST 4 // Reset pin (could connect to RST pin)
#define TFT_RST -1 // Set TFT_RST to -1 if display RESET is connected to ESP32 board RST

and I have uncommented in file TFT_eSPI/User_Setup_Select.h
#include <User_Setups/Setup70b_ESP32_S3_ILI9341.h> // Setup file for ESP32 S3 with SPI ILI9341

and flashed to esp32s3 and esp32s3 panics and contines to reboot again and again

please let me know what I am doing wrong

-Thanks
-Alok