ESP32S3 Battery Charging Problem

Hi there,

So, I think you misunderstood the WiKi “Battery Section”
, a LiPo battery is not a standalone lithium battery, but a type of lithium-ion battery

from the WiKi …

If you want to connect the battery for XIAO, we recommend you to purchase qualified rechargeable 3.7V lithium battery

Lithium battery vs. Li-Po, YMMV :crossed_fingers:

HTH
GL :slight_smile: PJ :v:

FYI , charge current is 51ma.
To find the charging time (T) you can use the formula that relates capacity and current
T=C/I

𝑇=2000mAh @51mA

T≈39.22 hourscap T is approximately equal to 39.22 hours

𝑇≈39.22 hours

That’s a long time to charge… :face_with_peeking_eye: I would re-evaluate your plan go for some deep sleep on a smaller battery. What is the App?