ESP32 Guide 2026

Two years ago, we looked at the state of the ESP32 family of microcontrollers. Well, a lot has changed since then - more ESP32 boards, more protocols, and 5 GHz Wi-Fi.

So here it is - the updated 2026 version of the ESP32 Guide.

We will begin by going over the different ESP32 variants; there are eleven of them, each with a unique set of features. Selecting the right one is vital to your project, and you can get more information and a downloadable spreadsheet on the article at https://dronebotworkshop.com/esp32-2026/

Then we will look at boards, broken down into the following categories:

  • General Purpose / Experimenter Boards

  • Display & Multimedia Boards

  • Compact & Portable Boards

  • IoT & Smart Home Boards

  • Budget & Starter Boards

  • Unique Boards

This should help you pick out the best ESP32 for your application.

1 Like