ERROR: sx1250 Image Calibration Error

I’m having trouble setting up my LoRaWAN module (WM1302) with my BeagleBone. I’ve connected everything, but I keep getting these errors:
ERROR: sx1250 Image Calibration Error
ERROR: radio calibration failed
ERROR: radio calibration failed
ERROR: [main] failed to start the concentrator
using the sx1302_hal library as per guidance of seeed studio LoRaWAN® Gateway Module WM1302 | Seeed Studio Wiki
configure the those pin on beagle bone :

Current mode for P9_17 is: spi_cs

Current mode for P9_21 is: spi

Current mode for P9_18 is: spi

Current mode for P9_22 is: spi_sclk

Current mode for P9_11 is: gpio (reset pin)

but I’m still facing the same issue.I don’t know what is going wrong.

Is it a Green one? Try switching P9_21 & P9_18
HTH
GL :slight_smile: PJ

what is HTH…? Helping he Hopeless…

New error arise beagle bone with communicate the lorawan(1302)

strong text
ERROR: Failed to set SX1250_0 in STANDBY_RC mode
ERROR: failed to setup radio 0
ERROR: [main] failed to start the concentrator

same configuration as previous post ,so what exact issue ?

it’s not green is industrial (black)