When I check the I2C connection between my raspberry pi and SHT35 using i2cdetect, it showed the address of the sensors. Therefore, I run my code and it works perfectly. However, when come to certain period, an error suddenly pop out and indicate “Errno 121”. Image below showed the error message.
Hi there~
We suspect the sensor lost connection with raspberry pi. I simulate it around 30 mins without issue.

</s>Relative Humidity is 53.49 %
Temperature in Celsius is 28.87 C
Relative Humidity is 53.40 %
Temperature in Celsius is 28.87 C
Relative Humidity is 53.38 %
Temperature in Celsius is 28.87 C
Relative Humidity is 53.56 %
Temperature in Celsius is 28.86 C
Relative Humidity is 53.87 %
Temperature in Celsius is 28.87 C
Relative Humidity is 53.96 %
Temperature in Celsius is 28.86 C
Relative Humidity is 53.80 %
Temperature in Celsius is 28.82 C
Relative Humidity is 53.72 %
Temperature in Celsius is 28.81 C
Relative Humidity is 53.73 %
Temperature in Celsius is 28.81 C
Relative Humidity is 53.73 %
Temperature in Celsius is 28.79 C
Relative Humidity is 53.82 %
Temperature in Celsius is 28.78 C
Relative Humidity is 53.83 %
Temperature in Celsius is 28.79 C
Relative Humidity is 53.81 %
Temperature in Celsius is 28.81 C
Relative Humidity is 54.06 %
Temperature in Celsius is 28.82 C
Relative Humidity is 54.31 %
Temperature in Celsius is 28.82 C
Relative Humidity is 54.43 %
Temperature in Celsius is 28.81 C
Relative Humidity is 54.48 %
Temperature in Celsius is 28.83 C
Relative Humidity is 54.72 %
Temperature in Celsius is 28.81 C
Relative Humidity is 55.20 %
Temperature in Celsius is 28.82 C
Relative Humidity is 54.98 %
Temperature in Celsius is 28.82 C
Relative Humidity is 54.59 %
Temperature in Celsius is 28.79 C
Relative Humidity is 54.33 %
Temperature in Celsius is 28.79 C
Relative Humidity is 54.36 %
Temperature in Celsius is 28.82 C
Relative Humidity is 54.17 %
Temperature in Celsius is 28.81 C
Relative Humidity is 54.07 %
Temperature in Celsius is 28.81 C
Relative Humidity is 53.95 %
Temperature in Celsius is 28.82 C
Relative Humidity is 53.81 %
Temperature in Celsius is 28.83 C
Relative Humidity is 53.73 %
Temperature in Celsius is 28.81 C
Relative Humidity is 53.67 %
Temperature in Celsius is 28.82 C
Relative Humidity is 53.60 %
<e>
If i unplug the sensor, it will show up the error121. please check your connection. thanks.
</s>Relative Humidity is 53.62 %
Traceback (most recent call last):
File "grove_I2C_High_Accuracy_tem_hum_SHT35_sensor.py", line 55, in <module>
main()
File "grove_I2C_High_Accuracy_tem_hum_SHT35_sensor.py", line 47, in main
temperature, humidity = sensor.read()
File "grove_I2C_High_Accuracy_tem_hum_SHT35_sensor.py", line 26, in read
self.bus.write_i2c_block_data(self.address, 0x24, [0x00])
File "/usr/local/lib/python2.7/dist-packages/smbus2/smbus2.py", line 482, in write_i2c_block_data
ioctl(self.fd, I2C_SMBUS, msg)
IOError: [Errno 121] Remote I/O error
<e>
Hi,
What make it suddenly lost connection from Pi. The error always shown up when I run about 6 hours.
Hi there~
Let’s keep running it tonight and see if any issue. thanks.