Erratic readings from Grove AC Voltage Sensor when mains not connected

Hi everyone,
I hope someone could share some insight.
I’d like to detect the presence of AC voltage (on or off, open or closed AC circuit) and chose this sensor as it’s a solid state solution. I’d love a relay, but don’t see a grove module with a relay that accepts 120 or 240 on the coil.

Basically, when I run the example “Voltage Sensing” and there is no input, the reading goes all over reading 1000 volts etc. Is this simply the wrong application?

Output from VoltageSensing from the library: GitHub - mcmchris/mcm-grove-voltage-sensor: AC analog voltage sensor module for energy monitoring.

Voltage: 825.19 V
Voltage: 792.47 V
Voltage: 789.68 V
Voltage: 814.82 V
Voltage: 592.79 V
Voltage: 701.92 V
Voltage: 567.02 V
Voltage: 484.95 V
Voltage: 394.74 V

My setup:

  • Seeedstudio Nano
  • Nano Grove Shield
  • Grove - AC Voltage Sensor (MCP6002)

I guess I somewhat expected that this unit would simply take RMS AC and scale it to 0-5 volts analog.

TLDR; I want to use the AC voltage sensor to check to see if there power, or there is no power. Instead, when no mains are connected, it reads erratically and would cause the Arduino to think that there is in fact power. Is there any way to fix this? Or is there a better solution on the Grove platform?

Thanks,
Roger

Hi there,
seems odd , but maybe you need a load in the circuit?
put a light in the circuit and see if it changes the readings?
HTH
GL :slight_smile: PJ

I have one setup that watches the 5V USB and if the charger is on(110v AC) if the usb is present, otherwise it’s off.
:v:

Hi,

The AC Voltage Sensor has been licensed to Seeed to manufacture and sell. Christopher Mendez will provide the tech support and Seeed will fulfill the order with hardware quality guaranteed.

If you need tech support you can contact Christopher with email [email protected].

@regor2 Did you solve this? I’m having the same sort of problem with 240V AC showing about 2500V when “on” and around 200V when “off” - this is using the default code from GitHub for the unit and an Arduino ESP32 Nano.

Nope, I moved on without finding a way- I wanted to find something withing the Grove ecosystem but ended up using a relay. If you find the solution, let us know :slight_smile: