That is, indeed, a Seeed display - SKU 104990843. On the Seeed page for that SKU there is an example listed, which is identical to the one listed on the ePaper Driver Board wiki except for:
- The Driver Board example pin definitions are updated for the XIAO D# scheme
- The Good Display version uses a 100,000 SPI bus
- The Good Display version shows a different test image
The Good Data example’s test image still renders with the same artifacts on the V2 board.