Hi,
I bought a Electronic brick - Electricity meter (Analog) recently and would like to use it. Can anyone help me with an example for Arduino?
MERRY CHRISTMAS
Ailton
Hi,
I bought a Electronic brick - Electricity meter (Analog) recently and would like to use it. Can anyone help me with an example for Arduino?
MERRY CHRISTMAS
Ailton
The electricity meter can used to measure the AC current through it , and it scale the AC current through it as 2000:1 and output , on the Electronic that this output current is by a resistor to change to voltage . so when 1A AC current through the electricity meter , the output voltage is about 400mV.
Hi,
I also recently bought this product, but without any docs or schematics its kind of hard to use…
For example:
Any help appreciated…
Thx, Goran
As expected then, but what value is the potentiometer? When measuring it, it seems to go from ca 150 ohm to ca 1050 ohm (if I remember correctly). Is there a 150 ohm resistor in series as well, built into the potentiometer?
Thx
-G