Hi I was wondering if that is possible to connect the EL shield to arduino Nano and if anyone can assist with the correct pin connections?
Hi,
Please find the schematic and board files in Wiki–>EL Shield. The pins mapped from Arduino to EL shield is available in schematic. The pin that are not connected can be made out from board layout.
The following screenshot of the layout shows which pins are connected.
Nano EL Shield(Marked on layout overlay)
-------------------------------------------------------------
GND GND
D7 D7 (CTL1)
D6 D6 (CTL2)
D5 D5 (CTL3)
D4 D4 (CTL4)
5V 5V
GND GND (Lower row pin headers)
VIN VIN
Let us know if the solution works.