Hello Everyone,
I’m trying to load a sketch that works fine on a nano, that writes an EEprom memory.
But I get this error:
C:\Users\focam\Documents\Arduino\libraries\Eeprom24C01_02-master\Eeprom24C01_02.cpp: In member function 'void Eeprom24C01_02::readBytes(byte, byte, byte*)':
C:\Users\focam\Documents\Arduino\libraries\Eeprom24C01_02-master\Eeprom24C01_02.cpp:52:35: error: 'BUFFER_LENGTH' was not declared in this scope
#define EEPROM__RD_BUFFER_SIZE BUFFER_LENGTH
^
C:\Users\focam\Documents\Arduino\libraries\Eeprom24C01_02-master\Eeprom24C01_02.cpp:219:33: note: in expansion of macro 'EEPROM__RD_BUFFER_SIZE'
byte bufferCount = length / EEPROM__RD_BUFFER_SIZE;
^~~~~~~~~~~~~~~~~~~~~~
C:\Users\focam\Documents\Arduino\libraries\Eeprom24C01_02-master\Eeprom24C01_02.cpp:52:35: note: suggested alternative: 'REG_DSU_LENGTH'
#define EEPROM__RD_BUFFER_SIZE BUFFER_LENGTH
^
C:\Users\focam\Documents\Arduino\libraries\Eeprom24C01_02-master\Eeprom24C01_02.cpp:219:33: note: in expansion of macro 'EEPROM__RD_BUFFER_SIZE'
byte bufferCount = length / EEPROM__RD_BUFFER_SIZE;
^~~~~~~~~~~~~~~~~~~~~~
C:\Users\focam\Documents\Arduino\libraries\Eeprom24C01_02-master\Eeprom24C01_02.cpp: In member function 'void Eeprom24C01_02::writePage(byte, byte, byte*)':
C:\Users\focam\Documents\Arduino\libraries\Eeprom24C01_02-master\Eeprom24C01_02.cpp:59:36: error: 'BUFFER_LENGTH' was not declared in this scope
#define EEPROM__WR_BUFFER_SIZE (BUFFER_LENGTH - 1)
^
C:\Users\focam\Documents\Arduino\libraries\Eeprom24C01_02-master\Eeprom24C01_02.cpp:255:33: note: in expansion of macro 'EEPROM__WR_BUFFER_SIZE'
byte bufferCount = length / EEPROM__WR_BUFFER_SIZE;
^~~~~~~~~~~~~~~~~~~~~~
C:\Users\focam\Documents\Arduino\libraries\Eeprom24C01_02-master\Eeprom24C01_02.cpp:59:36: note: suggested alternative: 'REG_DSU_LENGTH'
#define EEPROM__WR_BUFFER_SIZE (BUFFER_LENGTH - 1)
^
C:\Users\focam\Documents\Arduino\libraries\Eeprom24C01_02-master\Eeprom24C01_02.cpp:255:33: note: in expansion of macro 'EEPROM__WR_BUFFER_SIZE'
byte bufferCount = length / EEPROM__WR_BUFFER_SIZE;
^~~~~~~~~~~~~~~~~~~~~~
exit status 1
Errore durante la compilazione per la scheda Seeeduino XIAO.
Can anyone help me?