All:
Here’s the way to edit the CONTACTS list in the RePhone:
- Connect to a PC or Mac via the USB port (with the battery attached).
- Put the phone module into Mass Storage mode by holding down the reset button for 2 seconds.
- This should cause the phone to be mounted as a USB storage device.
Look for the file “contacts.txt” and edit using the format:
“Name, Phone Number”
such as
myfriend,5555551212
Got this by reading Rephone Kit manual & the article about using the Rephone with the Mac:
github.com/Seeed-Studio/CodeLit … n-Mac-OS-X
Charlie in Houston