EdgeBox RPI4 WM1302 issues

I am following section 3.3 of the EdgeBox user manual for the WM1302 installed in the Mini-PCIe and am using pin 5 for sx1302 reset and pin 6 for sx1302 power enable. I have already tested the WM1302 using a seeed Pi hat and a RPi4 per the wiki at LoRaWAN® Gateway Module WM1302 - Seeed Wiki and it works as described to start the LoRa packet forwarder. Now I am trying to do the same test using the EdgeBox RPi 200 with the WM1302 module installed in the EdgeBox. I have modified the reset_lgw.sh script to use pin 5 for sx1302 reset and pin 6 for sx1302 power enable. Following the instructions in the WM1302 wiki to start the packet forwarder using command “./lora_pkt_fwd -c global_conf.json.sx1250.US915” I get the error “ERROR: [main] failed to start the concentrator”. Can you provide any information or guidelines on how to use the WM1302 when installed in the EdgeBox? The only information on the seeed EdgeBox website for LoRa states “Mini-PCIe support LoRaWAN(Seeed WM1302 tested)*” and “You can use Seeed WM1302 module for LoRaWAN applications”. Is there any additional information or guidelines on using the EdgeBox with LoRa that can be provided?